I am running mainline kernel 4.2.6 on hummingboard-gate (imx6solo).
Now I have one raspberryPI as SPI master and the hummingboard as slave.
I connected SS/SCLK/MISO/MOSI, the waveform looks correct, however I never see data ready bit set in imx6's spi status register, or irq triggered.
all four pins are setup in IOMUXC as in pinmux tool.
ECSPI2 registers:
ECSPI_CONREG=0x00700001
ECSPI_CONFIGREG=0x000f0000
ECSPI_INTREG=0x00000008
CCM's ecspi2 clk is enabled, irq requested is 64
spi master is configured as CS active low, mode 0.
do I need to setup anything else?
已解决! 转到解答。
Hi Hongfeng
one can try patch
http://lkml.iu.edu/hypermail/linux/kernel/1509.3/01176.html
or port older kernel patch
https://community.freescale.com/docs/DOC-97380
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Hongfeng
one can try patch
http://lkml.iu.edu/hypermail/linux/kernel/1509.3/01176.html
or port older kernel patch
https://community.freescale.com/docs/DOC-97380
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
hi igorpadykov
Is it possible to apply this patch to linux-3.10 for adding Spi slave mode ?
I applied below path to linux-3.10 but, My imx6sx is not working as spi slave mode becaues spi rx isr doesn't get RX data.
i.MX6 ESPI slave mode support patch based on rel_imx_3.0.35_4.1.0
if you have any tip, please know to me.
I applied the patches in
Now the hummingboard is able to receive data from SPI.
thanks for the help!