imx6 sololite UART tx line activity while just receiving data

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6 sololite UART tx line activity while just receiving data

691 次查看
jagsgediya
Contributor II

Hi All,

We have a custom board based on the imx6 sololite.

We are facing the problem with the uart. We are just trying to receive the data through uart but when we are probing the Tx line, we are getting some garbage on it.

suppose I will do ,

cat /dev/ttymxc3

At this time also, I am getting some garbage on Tx line. Please help. What can be the reason?

Thanks,

Jags

标签 (4)
0 项奖励
2 回复数

518 次查看
igorpadykov
NXP Employee
NXP Employee

Hi jags

reason may be short circuit with another signals,

recommended to test hardware UART lines

with i.MX 6Series Platform SDK

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励

518 次查看
maitegonzalez
Contributor I

Hello,

We are working with a custom board also and we are facing the same issue..

Any solution?? 

Thanks!

Maite

0 项奖励