Dear All:
I have setup a rtsp server which can be play normally by others ARM platform , however, I got problem when I use imx6 android to play it.
my apk play the rtsp stream by the Android mediaplayer API.
Below is the logcat information:
V/EMemoryPower( 2534): VideoSequence----->0:0
I/caikq ( 2534): setVideoURI-------------------rtsp://admin:123456@192.168.0.123:554/mpeg4
I/caikq ( 2534): ----------------------------openvideo----------------------
V/VVV EVideoView( 2534): reset duration to -1 in openVideo
D/MediaPlayer( 2534): Couldn't open file on client side, trying server side
I/OMXPlayer( 2235): Loading content: rtsp://admin:123456@192.168.0.123:554/mpeg4
I/VVV EVideoView( 2534): 旧播放位置:-1------当前播放位置=0
E/tips ( 2594): id----->30
E/tips ( 2594): id----->35
I/OMXPlayer( 2235): LEVEL: 1 FUNCTION: InstanceInit LINE: 75
I/OMXPlayer( 2235): InitStreaming failed.
I/OMXPlayer( 2235): LEVEL: 1 FUNCTION: SysEventHandler LINE: 1336
I/OMXPlayer( 2235): OMX.Freescale.std.parser.streaming.sw-based report Error 80001020.
I/OMXPlayer( 2235): LEVEL: 1 FUNCTION: Load LINE: 598
I/OMXPlayer( 2235): Can't load content rtsp://admin:123456@192.168.0.123:554/mpeg4
I/OMXPlayer( 2235): Stop Player.
E/MediaPlayer( 2534): error (-2147483648, 0)
E/MediaPlayer( 2534): Error (-2147483648,0)
D/VVV EVideoView( 2534): Error: -2147483648,0
E/eten ( 2534): ------------------------播放出现错误-----------------
V/EMemoryPower( 2534): VideoSequence----->0:0
I/caikq ( 2534): setVideoURI-------------------rtsp://admin:123456@192.168.0.123:554/mpeg4
I/caikq ( 2534): ----------------------------openvideo----------------------
V/VVV EVideoView( 2534): reset duration to -1 in openVideo
D/MediaPlayer( 2534): Couldn't open file on client side, trying server side
I/OMXPlayer( 2235): Loading content: rtsp://admin:123456@192.168.0.123:554/mpeg4
the error information is report by the OMXPlayer.
pls help me to check out what problem occur in the OMXPlayer!
Thanks!
解決済! 解決策の投稿を見る。
Well, the error reported by the OMXPlayer is Error 80001020 which is OMX_ErrorFormatNotDetected. It means that the format of the input stream cannot be parsed or determined. However, this error seems to be happening AFTER an error from the MediaPlayer which seems to be while opening the file: D/MediaPlayer( 2534): Couldn't open file on client side, trying server side. So not sure ig the stream cannot be parsed because it is failing in first place to read the file. Are you sure the video file can be opened properly?
Well, the error reported by the OMXPlayer is Error 80001020 which is OMX_ErrorFormatNotDetected. It means that the format of the input stream cannot be parsed or determined. However, this error seems to be happening AFTER an error from the MediaPlayer which seems to be while opening the file: D/MediaPlayer( 2534): Couldn't open file on client side, trying server side. So not sure ig the stream cannot be parsed because it is failing in first place to read the file. Are you sure the video file can be opened properly?
Thanks for your reply, I'm sure the video url can be open, we setup the rtsp server and it has be tested in some arm platform