Hi all,
just testing some communications using PEAK usb CAN simulator.
I have seen that i can communicate up to 2Mbit/sec. Is this ok ?
With
ip link set can0 up type can bitrate 2000000
on both sides and using cangen tool.
Is it by the way this speed safe to be used ? At least, signals seems still good.
Hi Angelo
according to sect.26.1.2 FLEXCAN Module Features
i.MX 6Dual/6Quad Applications Processor Reference Manual
"..bit rate up to 1 Mb/sec"
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------