imx6: fingerprint as a Camera and ov5640 at the same board.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6: fingerprint as a Camera and ov5640 at the same board.

768 Views
fernando_mercad
Contributor II

Hi,

I´m using an imx6q with android Oreo 8.0 and I want to get a sensor fingerprint works as a Camera and the camera ov5640 without problems.

I mean:

## On Linux I have v4l2_cap_0 mapping the fingerprint to video0 and i2c-2, for the v4l2_cap_1 is mapping ov564x_mipi to video1 and i2c-0:

v4l2_cap_0 -----> video0 fingerprint ---------> i2c-2 (video0)

         |
imx6q-v4l2-capture


v4l2_cap_1 -----> video1 ov564x_mipi -------> i2c-0 (video1)
         |
imx6q-v4l2-capture

## In the device tree I have this:

i2c3 ------> fingerprint (csi_id = 0)
i2c1 ------> ov564x_mipi (csi_id = 1)

fingerprint -----> v4l2_cap_0 ------> csi_id = 0
ov5640 -----> v4l2_cap_1 ------> csi_id = 1

But I can´t get it works.

This is my output through ADB shell:

check:/ # dmesg | grep -i fingerprint
[ 1.852344] 0x000000000000-0x000000800000 : "fingerprint"
[ 2.568910] fingerprint : fingerprint _data.csi = [0]
[ 2.571703] Configuring fingerprint for 8-bit greyscale mode.
[ 2.660522] fingerprint : fingerprint _power: set power=1, current state=0
[ 2.665231] fingerprint : fingerprint  power On
[ 2.667596] fingerprint : fingerprint  reset
[ 2.751245] fingerprint : fingerprint _power: set power=0, current state=1
[ 2.755953] fingerprint : fingerprint  power Off
[ 2.780539] fingerprint : fingerprint _data.i2c_client->irq = [0]
[ 2.784465] fingerprint : fingerprint _data.i2c_client->name = [fingerprint]
[ 2.788997] camera fingerprint found
[ 11.950298] fingerprint : fingerprint _power: set power=1, current state=0
[ 11.955102] fingerprint : fingerprint  power On
[ 11.957469] fingerprint : fingerprint  reset
[ 12.040675] fingerprint : fingerprint _power: set power=0, current state=1
[ 12.045393] fingerprint : fingerprint  power Off

check:/ # dmesg | grep -i ov56
[ 2.791213] ov5640: ov5640_data.csi = [1]
[ 3.150545] ov5640: ov5640_data.i2c_client->irq = [0]
[ 3.154300] ov5640: ov5640_data.i2c_client->name = [ov564x_mipi]
[ 3.159006] camera ov5640_mipi is found

check:/ # dmesg | grep -i ipu
[ 0.499675] imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
[ 0.529667] imx-ipuv3 2800000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
[ 0.531016] IPU: gmipi_csi2->ipu_id = [0]
[ 0.531025] IPU: gmipi_csi2->csi_id = [1]

check:/ # dmesg | grep -i v4l2
[ 2.556801] mxc_v4l2_output v4l2_out: V4L2 device registered as video16
[ 2.562332] mxc_v4l2_output v4l2_out: V4L2 device registered as video17

check:/ # ls -lrat /dev/video*

crw-rw---- 1 system camera 81, 1 2019-01-07 17:03 /dev/video17
crw-rw---- 1 system graphics 81, 0 2019-01-07 17:03 /dev/video16
crw-rw-rw- 1 system camera 81, 3 2019-01-07 17:03 /dev/video1
crw-rw-rw- 1 system camera 81, 2 2019-01-07 17:03 /dev/video0

check:/ # ls -lrat /dev/i2c-*

crw-rw-rw- 1 system root 89, 2 2019-01-07 17:03 /dev/i2c-2
crw------- 1 root root 89, 1 2019-01-07 17:03 /dev/i2c-1
crw-rw-rw- 1 system root 89, 0 2019-01-07 17:03 /dev/i2c-0

We can see above, the two cameras are found, but when I start the default app for the camera I get; "Can´t connect to the camera". But the app for the fingerprint it works without problem.

Perhaps, with some "sepolicy" it could be resolve, however I'm not sure.

Can someone help me, or give some advice please?.

Regards,

Thanks.

Labels (4)
0 Kudos
2 Replies

545 Views
fernando_mercad
Contributor II

Hi Igor, 

About the commands, I can't try with these, cause my board is custom then it don't have those commands.

But, thanks so much for your help.

Do you know, What could I try more?

Regards.

0 Kudos

545 Views
igorpadykov
NXP Employee
NXP Employee

Hi Fernando

one can try to test it first on linux using commands provided on

i.mx6:two camera work at the same time 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos