imx6 android9.0 use sgtl5000 on HDMI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6 android9.0 use sgtl5000 on HDMI

883件の閲覧回数
minyou
Contributor II

Hello:

I want to ask!

On imx6 android 9.0, when I use HDMI, sgtl5000 has no sound effect. I should connect HDMI and switch to HDMI sound effect card.
Is there a patch that can output sound effects at the same time when HDMI sound card and sgtl5000 are connected?

タグ(4)
0 件の賞賛
返信
2 返答(返信)

864件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi minyou

 

sgtl5000 is not supported on nxp i.mx reference boards, one can look at third parties,

like sabrelite board:

https://github.com/boundarydevices/linux-imx6/blob/boundary-imx_5.4.x_2.1.0/arch/arm/boot/dts/imx6qd...

https://boundarydevices.com/android-oreo-8-0-0-release-for-i-mx6-boards/

 

Best regards
igor

0 件の賞賛
返信

861件の閲覧回数
minyou
Contributor II

Hi igor

sorry , I use imx6q, I can use sgtl5000 on android 6.0
I connected HDMI to android 6.0, my sound effect can be output from sgtl5000,
But I can’t let him output sound effects from sgtl5000 in HDMI mode on android9.0.
I am guessing whether it needs to be modified in tinyalsa_hw.c?

0 件の賞賛
返信