Hi,all!
I have a board based on i.MX6dl, with wm8960 chip connected to i2c1 and audmux3. With the uboot-2016.03, kernel-4.1.15 and rootfs, i can play wav files and record the voice from mic, it works well. And the above images are provided by the board vendor.
I built a rootfs with busybox, alsa-lib and alsa-utils, and i use it as the rootfs for the board, and i also rebuild the uboot and kernel with the same cross compile gcc toolchain. when i used aplay to play a wav file, it return an error message as follows:
/ # aplay abba_out.wav
Playing WAVE 'abba_out.wav' : Signed 16 bit Little Endian, Rate 22050 Hz, Stereo
aplay: pcm_write:1940: write error: Input/output error
But there was a time i can play the wav file with my own roofs, however i just forget the configuration and it never reappear again.
Is there any advice for that?
Thanks a lot.
Hi,
I am using imx8mp-evk. i am facing the same problem. when image built with yocto it works fine and i can play wav files, but when build my own rootfs it stoped working and it throwswrite error.
Any solution to this problem?
Regards
The latest progress is as follows
in pcm_lib.c wait_for_avail
tout = schedule_timeout(wait_time);
if (!tout) {
pcm_dbg(substream->pcm, "%s write error (DMA or IRQ trouble?)\n",
is_playback ? "playback" : "capture");
err = -EIO;
break;
}
And once i enabled the pcm_dbg output, the aplay will print "playback write error (DMA or IRQ trouble?)"
It seem like it was caused by DMA or IRQ ?
Hi chao
please look on
for building images use nxp linux sources and documentation from
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I use the strace tool to analysis the process of aplay.
And i find that after several times of snd_pcm_lib_write1 called successfully, in snd_pcm_lib_write1 function,
avail = snd_pcm_playback_avail(runtime);
avail = 0;
and it will use "err = wait_for_avail(substream, &avail);" to wait for avail, but it will return -5.
the return err leads to "aplay: pcm_write:2051: write error: Input/output error"
Thanks.
Hi igorpadykov
Thanks for your advice.
I've found the web pages before i posed the problem, which you listed. but i dont have any idea about the error.
It is so strange that i only changed the rootfs, and the kernel and the wm8960 driver should be ok, what i did is rebuild them with my gcc toolchain.
1、I use uboot and linux kernel images, which i rebuild, and the rootfs, provided by board vendor, i can excute aplay and arecord operation, it works well.
2、When i use my rebuilt rootfs to replace rootfs in step 1, the system startup successfully. But i can't play a wav file, it return Input/Output error.
When i play a wav file, it is stucked, and after a while, it returns "aplay: pcm_write:2051: write error: Input/output error"
And i checked the alsa-uitls/aplay/aplay.c, it seems that "snd_pcm_writei" return a minus.
The more detailed log is as follows:
/ # aplay -vv abba_out.wav
Playing WAVE 'abba_out.wav' : Signed 16 bit Little Endian, Rate 22050 Hz, Stereo
Plug PCM: Hardware PCM card 0 'wm8960-audio' device 0 subdevice 0
Its setup is:
stream : PLAYBACK
access : RW_INTERLEAVED
format : S16_LE
subformat : STD
channels : 2
rate : 22050
exact rate : 22050 (22050/1)
msbits : 16
buffer_size : 13780
period_size : 2756
period_time : 124988
tstamp_mode : NONE
tstamp_type : MONOTONIC
period_step : 1
avail_min : 2756
period_event : 0
start_threshold : 13780
stop_threshold : 13780
silence_threshold: 0
silence_size : 0
boundary : 1806172160
appl_ptr : 0
hw_ptr : 0
############# + | 30%aplay: pcm_write:2051: write error: Input/output error