imx6 SPI - Master Mode with Wait States

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 SPI - Master Mode with Wait States

990 Views
viniciusmaciel
Contributor II

Hi,

I did a little modification in spi-imx driver to insert 0 wait states in SCLK between data, but it is not working! I am using an imx6 wandboard board with kernel 4.9.11.

/* 0 wait states inserted */
 reg = readl(spi_imx->base + MX51_ECSPI_PERIOD);
 reg &= ~(MX51_ECSPI_PERIOD_MASK); // MASK=0x7FFF
 writel(reg, spi_imx->base + MX51_ECSPI_PERIOD);

There is still a 2.2uS delay.

Labels (1)
Tags (2)
0 Kudos
1 Reply

757 Views
igorpadykov
NXP Employee
NXP Employee

Hi Vinicuis

one can try to use larger burst lengths using the BURST_LENGTH
setting in register ECSPIx_CONREG and spi native chip select patch:

[2/2] spi: imx: fix use of native chip-selects with devicetree - Patchwork 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos