imx6 HDMI working status differed by cable plugging

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 HDMI working status differed by cable plugging

Jump to solution
1,552 Views
TKayO
Contributor III

Hello, 

My imx6qp board has HDMI, 

if my board powered with the HDMI port is plugged to a monitor, 

while Android booting, my monitor shows the framebuffer content and

plug & plug to other monitor also works well..

 

But my board boot up without plugging any HDMI cable, 

after booting is done, HDMI is not working.

Cable plugging event is active but no screen output on my monitor.

 

attached two different log

Please give me any hint.

 

Regards.

 

 

0 Kudos
1 Solution
1,480 Views
igorpadykov
NXP Employee
NXP Employee

please try to reproduce issue on NXP Sabre SD reference board with

Demo Image i.MX 6Quad, i.MX 6QuadPlus, and i.MX 6DualLite SABRE-AI

 

Best regards
igor

 

View solution in original post

0 Kudos
8 Replies
1,546 Views
igorpadykov
NXP Employee
NXP Employee

Hi WOOSEOK

 

what bsp used in the case, hdmi cable plugging issues were in old releases as reported for example on

https://www.yoctoproject.org/pipermail/meta-freescale/2014-July/009430.html

May be recommended to try latest nxp releases

https://www.nxp.com/design/software/embedded-software/i-mx-software/android-os-for-i-mx-applications...

 

Best regards
igor

0 Kudos
1,488 Views
TKayO
Contributor III

@igorpadykov Is that all?  since my recent updates, you didn't mentioned anything.. 

 

+

fb0 is for LCD, 

fb1 is for HDMI and boot param has info about it.

When cable is plugged, fb1 is reconfigured and done something about init. but

without cable, it's not. 

 

0 Kudos
1,481 Views
igorpadykov
NXP Employee
NXP Employee

please try to reproduce issue on NXP Sabre SD reference board with

Demo Image i.MX 6Quad, i.MX 6QuadPlus, and i.MX 6DualLite SABRE-AI

 

Best regards
igor

 

0 Kudos
1,465 Views
TKayO
Contributor III

Thank you for your concern

and sorry for my frequent questions.

it was a hardware problem.  there was no pull-up register for the HPD pin.

 

0 Kudos
1,524 Views
TKayO
Contributor III

also looks very similar with below issue

 

https://community.nxp.com/t5/i-MX-Processors/imx-hdmi-audio-HDMI-Video-is-not-ready/td-p/478851

 

but my kernel parameter contains 

"video=mxcfb0:dev=mipi_dsi,ST7703-HD,if=RGB24 video=mxcfb1:dev=hdmi,1920x1080M@60,if=BGR24"

 

0 Kudos
1,534 Views
TKayO
Contributor III

Dear Igor, 

Also you can see from my attachments, 

When I power up my board without HDMI cable plugged, below error message occurs.

 

[ 17.976039] imx-hdmi-audio imx-hdmi-audio: HDMI Video is not ready!
[ 17.981175] imx-hdmi-audio imx-hdmi-audio: ASoC: can't open platform imx-hdmi-audio: -22
[ 17.988414] imx-hdmi-audio imx-hdmi-audio: HDMI Video is not ready!
[ 17.993415] imx-hdmi-audio imx-hdmi-audio: ASoC: can't open platform imx-hdmi-audio: -22

 

Thank you

0 Kudos
1,539 Views
TKayO
Contributor III

FYI, my android bsp version is "p9.0.0_2.2.0-ga"

0 Kudos
1,540 Views
TKayO
Contributor III

Thank you for your reply Igor, 

But my case is opposite, HDMI works only when the cable is plugged at the time power enabled.

After boot up, then I plug the cable, there's no EDID handshaking happens and no display at all.

 

0 Kudos