Hello,
My imx6qp board has HDMI,
if my board powered with the HDMI port is plugged to a monitor,
while Android booting, my monitor shows the framebuffer content and
plug & plug to other monitor also works well..
But my board boot up without plugging any HDMI cable,
after booting is done, HDMI is not working.
Cable plugging event is active but no screen output on my monitor.
attached two different log
Please give me any hint.
Regards.
解決済! 解決策の投稿を見る。
please try to reproduce issue on NXP Sabre SD reference board with
Demo Image i.MX 6Quad, i.MX 6QuadPlus, and i.MX 6DualLite SABRE-AI
Best regards
igor
Hi WOOSEOK
what bsp used in the case, hdmi cable plugging issues were in old releases as reported for example on
https://www.yoctoproject.org/pipermail/meta-freescale/2014-July/009430.html
May be recommended to try latest nxp releases
Best regards
igor
@igorpadykov Is that all? since my recent updates, you didn't mentioned anything..
+
fb0 is for LCD,
fb1 is for HDMI and boot param has info about it.
When cable is plugged, fb1 is reconfigured and done something about init. but
without cable, it's not.
please try to reproduce issue on NXP Sabre SD reference board with
Demo Image i.MX 6Quad, i.MX 6QuadPlus, and i.MX 6DualLite SABRE-AI
Best regards
igor
Thank you for your concern
and sorry for my frequent questions.
it was a hardware problem. there was no pull-up register for the HPD pin.
also looks very similar with below issue
https://community.nxp.com/t5/i-MX-Processors/imx-hdmi-audio-HDMI-Video-is-not-ready/td-p/478851
but my kernel parameter contains
"video=mxcfb0:dev=mipi_dsi,ST7703-HD,if=RGB24 video=mxcfb1:dev=hdmi,1920x1080M@60,if=BGR24"
Dear Igor,
Also you can see from my attachments,
When I power up my board without HDMI cable plugged, below error message occurs.
[ 17.976039] imx-hdmi-audio imx-hdmi-audio: HDMI Video is not ready!
[ 17.981175] imx-hdmi-audio imx-hdmi-audio: ASoC: can't open platform imx-hdmi-audio: -22
[ 17.988414] imx-hdmi-audio imx-hdmi-audio: HDMI Video is not ready!
[ 17.993415] imx-hdmi-audio imx-hdmi-audio: ASoC: can't open platform imx-hdmi-audio: -22
Thank you
FYI, my android bsp version is "p9.0.0_2.2.0-ga"
Thank you for your reply Igor,
But my case is opposite, HDMI works only when the cable is plugged at the time power enabled.
After boot up, then I plug the cable, there's no EDID handshaking happens and no display at all.