imx53 WEC7 LOGO

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx53 WEC7 LOGO

2,092 次查看
lee_ee
Contributor II

Hi

I want to remove the WEC7 startup picture that Eboot running later appear block MS logo with black background,

What should I do?

Thanks

7 回复数

1,497 次查看
wangyx
Contributor III

have you tried replace the  windowsce.png pic. in the directory FILES ? Then build . Try it.

0 项奖励
回复

1,497 次查看
SergioSolis
NXP Employee
NXP Employee

To replace the splash screen logo with your own you need platform builder to recompile the bootloader to get the custom image embedded in the code. The logo image code is BOOTLOADER\Display\bsp_logo.c

1,497 次查看
lee_ee
Contributor II

thanks serchMX

It's not splash screen logo, it's microsoft WEC logo as follows:0_1331620334V4vo.gif

I want not display it when OS boot up

0 项奖励
回复

1,497 次查看
Oceanblue
Contributor III

Does anyone know what Wifi module can run on MX53 WinCE7 platform? thx

Jack

0 项奖励
回复

1,497 次查看
holyyuan
Contributor II

I once added the WiFi function on IMX53 SMD WinCE7 OS. In the Catalog Item, choose CoreOS ->Windows Embedded Compact-> Shell and User Interface -> User Interface ->WiFi setting, then Rebuild the BSP and get the new kernel.After burn the kernel into the SDMMC, power on the platform in control  panel ,can find the corresponding settings.   But now cannot remember so clearly. so you may have a try!

0 项奖励
回复

1,497 次查看
Oceanblue
Contributor III

Holy, thanks for comment, could you please indicate what WIFI module you have tested? you know currently it's difficult to get Wifi module to support WinCE7. thx.

0 项奖励
回复

1,497 次查看
embwise
Contributor I

Please check out http://www.embwise.com - they provide WIFi drivers for WEC7.

0 项奖励
回复