imx51 wince6 start slow from sdmmc

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imx51 wince6 start slow from sdmmc

跳至解决方案
1,094 次查看
lee_ee
Contributor II

Dear all
I working on imx51 wince6,OS is boot from eMMC(8G inand),but the system start up consume long time

I follow the debug log to find that OS run OAL layer RTC reset,stop here for long time.

what reason lead to OS start so slow ?

Thanks ahead

0 项奖励
1 解答
937 次查看
justin_jiang
NXP Employee
NXP Employee

Hi Lee_ee,

Since we didn't add log after RTC reset, so you will see it stop on it. Actually it may cost some time on one driver loader. Please add more log on each driver initial function to check which driver cost so long time for boot.

在原帖中查看解决方案

0 项奖励
2 回复数
938 次查看
justin_jiang
NXP Employee
NXP Employee

Hi Lee_ee,

Since we didn't add log after RTC reset, so you will see it stop on it. Actually it may cost some time on one driver loader. Please add more log on each driver initial function to check which driver cost so long time for boot.

0 项奖励
937 次查看
lee_ee
Contributor II

thanks

0 项奖励