imx283 + linux-fslc 5.4-2.3.x-imx: use of non-existent IP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx283 + linux-fslc 5.4-2.3.x-imx: use of non-existent IP

612 Views
pty
Contributor I

This commit on 5.4-2.3.x-imx introduces the use of EPDC that is (at least) undocumented in MCIMX28RM.pdf (i.MX28 Reference Manual). I don't believe it has an undocumented EPDC IP inside though.

Newer SoCs like i.MX6 and i.MX8 have EPDCs implemented and their LCDIF version is 4. LCDIF on i.MX28 is also version 4 and the comparison of IP version can accidentally cause access to non-existent registers.

Should I patch the lines to remove EPDC-related lines if I use 5.4-2.3.x-imx on i.MX28?

Labels (1)
0 Kudos
1 Reply

591 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello pty,

 

The latest linux BSP available is kernel 2.6.35, this is very old and is not recommended for new design. if you are on 5.4.2 this is the community bsp and is not supported by nxp. So please go the community.

Regards

 

0 Kudos