imx28 i2c timing issue with optimization flag

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx28 i2c timing issue with optimization flag

1,306件の閲覧回数
shashikanthirem
Contributor III

Hi All,

I am using i2c send and receive written local i2c function call, which am seeing a I2C querry success and perfectly when I enable optimization(-O0) debug symbols, but does not works(NACK) when i remove the above (-O0)  compiler from the Makefie.

Any suggestion would be helpful

using 

linux 2.635.3, LTIB

ラベル(2)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

1,161件の閲覧回数
shashikanthirem
Contributor III

pastedImage_1.png

pastedImage_2.png

0 件の賞賛
返信

1,161件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi shashikant

one can look at attached documentation about new ltib toolchain

and test if this helps.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,161件の閲覧回数
shashikanthirem
Contributor III

i cannot do as of now.. 

0 件の賞賛
返信