As i'm using a nand flash to boot and it requests a reset command before any read/write command.
My question is how to control the NF_BOOT_WITH_RESET signal? Should I use a pin at boot? Should I use a bit of the fusebox?
解決済! 解決策の投稿を見る。
The i.MX25 external (direct) boot is affected by the (RESET -0xFF) issue,
which means - no reset command (0xFF) is issued before boot.
In this case, please use internal boot, when the i.MX25 internal bootloader
issues the NAND reset command (0xFF) as first command after power up during NAND
boot.
Also note, ONFI NANDs have a timeout behavior : even if it hasn't received the
0xFF reset command, after timeout it will also be ready for access.
So, power up delay between NAND is powered on and IMX25 starts NAND access may
be used as a workaround.
In the same time the i.MX25 internal (ROM) bootloader issues the NAND reset
command (0xFF) as first command after power up during NAND boot.
This means only internal boot mode of the i.MX25 should be used.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
The i.MX25 external (direct) boot is affected by the (RESET -0xFF) issue,
which means - no reset command (0xFF) is issued before boot.
In this case, please use internal boot, when the i.MX25 internal bootloader
issues the NAND reset command (0xFF) as first command after power up during NAND
boot.
Also note, ONFI NANDs have a timeout behavior : even if it hasn't received the
0xFF reset command, after timeout it will also be ready for access.
So, power up delay between NAND is powered on and IMX25 starts NAND access may
be used as a workaround.
In the same time the i.MX25 internal (ROM) bootloader issues the NAND reset
command (0xFF) as first command after power up during NAND boot.
This means only internal boot mode of the i.MX25 should be used.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------