Hi,
I have a custom board with an imx233 BGA and 2 chip of ram 64MB (one wired on each chip select).
Linux boots correctly on it.
The problem I have is whatever I do u-boot says I have only 64MB of RAM, but I should have 128MB. Do you know if there is any software adjustments to do so that it can work?
Thank you in advance,
Regards,
Pierre.
解決済! 解決策の投稿を見る。
Pierre,
mx23evk detects 128MB correctly. You may need to adapt this following commit into your board:
commit 920178d38133e76da8b0394b0d3f088e7afbaee7
Author: Otavio Salvador <otavio@ossystems.com.br>
Date: Sat Feb 23 02:43:06 2013 +0000
mx23evk: Adjust DRAM control register to use full 128MB of RAM
Adjust HW_DRAM_CTL14 to enable the chip selects to allow usage of full
128MB of RAM.
Signed-off-by: Otavio Salvador <otavio@ossystems.com.br>
diff --git a/board/freescale/mx23evk/spl_boot.c b/board/freescale/mx23evk/spl_bo
index 6007433..b6f4e7e 100644
--- a/board/freescale/mx23evk/spl_boot.c
+++ b/board/freescale/mx23evk/spl_boot.c
@@ -98,6 +98,16 @@ const iomux_cfg_t iomux_setup[] = {
(MXS_PAD_4MA | MXS_PAD_3V3 | MXS_PAD_NOPULL),
};
+#define HW_DRAM_CTL14 (0x38 >> 2)
+#define CS_MAP 0x3
+#define INTAREF 0x2
+#define HW_DRAM_CTL14_CONFIG (INTAREF << 8 | CS_MAP)
+
+void mxs_adjust_memory_params(uint32_t *dram_vals)
+{
+ dram_vals[HW_DRAM_CTL14] = HW_DRAM_CTL14_CONFIG;
+}
+
void board_init_ll(void)
{
mxs_common_spl_init(iomux_setup, ARRAY_SIZE(iomux_setup));
By the way:
Did anyone test u-boot with the evaluation kit? Did u-boot detect that there was 2 rams and 128MB?
(There might very well be an electronic problem on our board, but it seems strange because everything else works fine)
I'm just reading the freescale doc it says:
The number of connected chip selects and their connection orientation is based on the programming in
the HW_DRAM_CTL14_CS_MAP bit field. Because the internal DRAM controller supports up to 4
memory chips, this field is structured to support either one, two, or four memory chips. However, because
only 2 memory chip selects are pinned out on the 169BGA package and only 1 memory chip select is
pinned out on the 128QFP package, not all CS_MAP configurations can be used.
Below are examples of valid system configurations for the CS_MAP bit field:
•
CS_MAP = b0001: One memory device is connected to EMI_CE0n (configuration supported in
128LQFP and 169BGA).
•
CS_MAP = b0010: One memory device is connected to EMI_CE1n (configuration supported in
169BGA only).
•
CS_MAP = b0011: Two memory devices are connected - one to EMI_CE0n and one to
EMI_CE1n. (configuration supported in 169BGA only).
So it seems that a register needs to be configured, doesn't it?
Pierre,
mx23evk detects 128MB correctly. You may need to adapt this following commit into your board:
commit 920178d38133e76da8b0394b0d3f088e7afbaee7
Author: Otavio Salvador <otavio@ossystems.com.br>
Date: Sat Feb 23 02:43:06 2013 +0000
mx23evk: Adjust DRAM control register to use full 128MB of RAM
Adjust HW_DRAM_CTL14 to enable the chip selects to allow usage of full
128MB of RAM.
Signed-off-by: Otavio Salvador <otavio@ossystems.com.br>
diff --git a/board/freescale/mx23evk/spl_boot.c b/board/freescale/mx23evk/spl_bo
index 6007433..b6f4e7e 100644
--- a/board/freescale/mx23evk/spl_boot.c
+++ b/board/freescale/mx23evk/spl_boot.c
@@ -98,6 +98,16 @@ const iomux_cfg_t iomux_setup[] = {
(MXS_PAD_4MA | MXS_PAD_3V3 | MXS_PAD_NOPULL),
};
+#define HW_DRAM_CTL14 (0x38 >> 2)
+#define CS_MAP 0x3
+#define INTAREF 0x2
+#define HW_DRAM_CTL14_CONFIG (INTAREF << 8 | CS_MAP)
+
+void mxs_adjust_memory_params(uint32_t *dram_vals)
+{
+ dram_vals[HW_DRAM_CTL14] = HW_DRAM_CTL14_CONFIG;
+}
+
void board_init_ll(void)
{
mxs_common_spl_init(iomux_setup, ARRAY_SIZE(iomux_setup));
Ok I see thanks!
I added this patch to my u-boot config it now says that I have ... 16MB of ram! What?
I'm going to try with a cleaner u-boot version because the one I use is a little dirty...
Even with a clean u-boot from git repository with imx23evk_config I get 16MiB of ram, very strange...
Might be an electronic problem, then I guess...
Ok it works! :smileyhappy: 128mio!
So at first I had a u-boot configuration problem as you pointed out.
I had also a small solder bridge which prevented the second ram to work. Now it's fine!
Hi Pierre
in uboot2009.08 one can check parameters in include/configs/mx23_evk.h :
#define CONFIG_NR_DRAM_BANKS |
#define PHYS_SDRAM_1 |
#define PHYS_SDRAM_1_SIZE
Best regards
igor
Thanks for the answer.
Here is what I have:
#define CONFIG_NR_DRAM_BANKS | 1 | /* 1 bank of DRAM */ |
#define PHYS_SDRAM_1 | 0x40000000 /* Base address */ | |
#define PHYS_SDRAM_1_SIZE | 0x08000000 /* Max 128 MB RAM */ | |
#define CONFIG_SYS_SDRAM_BASE |
Is it correct?