[Apologies for not formatting this well - I haven't yet figured out how to turn text into a code block...]
I'm trying to migrate from MfgTool on Windows to imx_usb_loader (+ utp_com) on Linux.
My board uses a i.MX6 Solo SOM, with the u-boot supplied (and modified!) by the SOM manufacturer. I have though got this working with MfgTool (even with a signed u-boot and a secured cpu). So I'm pretty confident that my images are all 'good'.
I've got as far as the mfg u-boot booting, but it seems to rely on having its environment downloaded too - the MfgTool xml includes the entry:
<CMD state="BootStrap" type="load" file="mfg.env" address="0x10500000" loadSection="OTH" setSection="OTH" HasFlashHeader="FALSE" >Loading mfg U-Boot parameters.</CMD>
I've added this to the .conf file for imx_loader, which so far has:
mx6_qsb
hid,1024,0x910000,0x10000000,1G,0x00907000,0x31000
firmware/mfg.env: load 0x10500000
firmware/u-boot-tx6s-8035_mfg.bin:clear_dcd,load,plug,jump header, load 0x14f0000
As I say, u-boot starts, but crashes when trying to write the env. With MfgTool it shows:
## Warning: defaulting to text format
## Info: input data size = 1575 = 0x627
Saving Environment to MMC...
whereas with imx_usb_loader I'm getting:
## Warning: defaulting to text format
## Info: input data size = 787451 = 0xC03FB
then one of a few errors/crashes.
Note that, even with a power-cycle, it seems to consistently come up with 787451
I've enabled some debug, which for this stage shows:
== work item
filename firmware/mfg.env
load_size 0 bytes
load_addr 0x10500000
dcd 0
clear_dcd 0
plug 0
jump_mode 0
jump_addr 0x00000000
== end work item
load_addr=10500000
loading binary file(firmware/mfg.env) to 10500000, skip=0, fsize=2b3 type=0
<<<691, 1024 bytes>>>
succeeded (status 0x88888888)
Am I correct in using that 'load' entry to send the env?
What's the significance of the fist line of the conf ("mx6_qsb") - not sure if I should change this?
Any suggestions please on what could be wrong?
Thanks.
已解决! 转到解答。
Ok, I've sorted that: there's two env files that the mfg u-boot needs downloading - one @ 0x10500000 and another @ 0x10540000. And, both have to include a null at the end - the u-boot image parses the data as strings and then saves the total environment to MMC.
Now getting as far as the mfg kernel booting up with the initramfs - onward now to partitioning and downloading the production images...!
in general issues with imx_usb_loader may be debugged using its sources
GitHub - boundarydevices/imx_usb_loader: USB & UART loader for i.MX5/6/7 series
Best regards
igor
Very shabby replying to my own post.... but I've just noticed that the working MfgTool boot is saying
"Info: input data size = 1575 = 0x627"
when the size of the file is (and also as reported by imx_usb_loader) in fact 691 bytes...?
Ok, I've sorted that: there's two env files that the mfg u-boot needs downloading - one @ 0x10500000 and another @ 0x10540000. And, both have to include a null at the end - the u-boot image parses the data as strings and then saves the total environment to MMC.
Now getting as far as the mfg kernel booting up with the initramfs - onward now to partitioning and downloading the production images...!