imx platform is not rebooting

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx platform is not rebooting

1,035 次查看
mutyalaraoneela
Contributor III

Hi All,

Platform: imx6sololite

kernel : 3.10.17

I have cross compiled my wlan driver and installed on the platfrom, As a client after connecting to the Access Point, after successful connection and short ping when I execute "reboot" command, platform is not rebooting. I need to hard reset it (ie..Press button on the platform).

Observation: No crashes and no hanging after installing the driver.

Please help me to move forward.

Thanks and Regards,

Mutyalarao.

标签 (4)
0 项奖励
回复
2 回复数

865 次查看
igorpadykov
NXP Employee
NXP Employee

Hi mutyalarao

one can refer to i.MX6SL Linux EVK Release Notes p.8

Table 8 Known Issues and Workarounds :

"Reboot may not work on EVK board."

that is recommendation is to assert pmic reset (PWRON), resetting whole board.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

865 次查看
mutyalaraoneela
Contributor III

Hi Igor,

Thank you for your quick reply.

Are the known issues going to be fixed in the next version of boards?

0 项奖励
回复