iMXRT-1064; booting directly to active firmware in internal FLASH

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMXRT-1064; booting directly to active firmware in internal FLASH

跳至解决方案
760 次查看
jaripeltonen
Contributor IV

Hello!

I'm working on a project where we use iMXRT-1064. I have a question regarding Firmware swap feature that is introduced in document AN12255 and AN12240. This question is also linked to discussion thread on the same topic (https://community.nxp.com/t5/i-MX-RT/iMXRT1064-Issue-with-firmware-swap/m-p/1345041#M16437)

The question is; Is it possible to set iMXRT-1064 to automatically boot directly to a predefined (active) FLASH section, so that the API function call "bl_firmware_switch()" would not be needed?

An example; the internal FLASH is divided into two 2 MByte sections (0 and 1), and the active (latest) firmware has been programmed into section 1 (address 0x7020 0000). Now, the device boots up on section 0 (0x7000 0000) and from there we have to jump to section 1 in order to run the latest SW image. Is there any way to make the processor to boot directly from section 1 so that the jump command would not be needed?

Thanks & best regards,

Jari

标签 (1)
0 项奖励
1 解答
751 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Is it possible to set iMXRT-1064 to automatically boot directly to a predefined (active) FLASH section, so that the API function call "bl_firmware_switch()" would not be needed?
-- No, I'm afraid not
Have a great day.
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
2 回复数
752 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Is it possible to set iMXRT-1064 to automatically boot directly to a predefined (active) FLASH section, so that the API function call "bl_firmware_switch()" would not be needed?
-- No, I'm afraid not
Have a great day.
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
746 次查看
jaripeltonen
Contributor IV

Hi Jeremy,

Thanks for your fast reply!

I will close this thread as I have no further questions.

Best regards,

Jari

0 项奖励