iMX93 EVK Porting USB Hub to replace USB Type-C

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX93 EVK Porting USB Hub to replace USB Type-C

120 Views
AlanWen
Contributor III

imx-manifest version: imx-6.6.3-1.0.0

Board: i.MX93 EVK

I'm trying to build the USB 2.0 Hub on customized board, but the original i.MX93 EVK board only have two USB type-c in device tree at

imx93evk_build/tmp/work/imx93evk-poky-linux/u-boot-imx/2023.04/git/arch/arm/dts/imx93-11x11-evk.dts

How can I edit the device tree & configurations to build USB 2.0 Hub to replace the original type-c ?

 

BR

Alan

0 Kudos
1 Reply

99 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

You can edit the dtb as you want, you just go to $WORKDIR/kernel/build/arch/arm/boot/dts/  and edit it.

regards

0 Kudos