iMX8QM USB REXT pull-down

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8QM USB REXT pull-down

1,279 Views
pbain
Contributor III

Hi guys, there is a pull-down resistor required on both USB_OTG2_REXT and USB_SS3_REXT.

Technical Datasheet (Rev 0, 10/2019) page 83 specifies 500R 0.5% (497.5Ω to 502.5Ω).
Hardware Developers Guide (v0.6, 01/2019) page 20 specifies 499R 1% (494Ω to 504Ω)

I don't think this is going to be an issue, but thought I would ask anyway to clarify which is correct and to let you know that the documentation should be changed to agree with each other.

Regards,

Peter

Tags (2)
0 Kudos
Reply
2 Replies

1,223 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  Use the recent Datasheet(s)  with hardware specs.

i.MX 8 Family Applications Processor | Arm Cortex-A53/A72/M4 | NXP 

   Note, the HDG is not published yet.

Have a great day,

Yuri

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 Kudos
Reply

573 Views
a_harr
Contributor II

@Yuri: In the meantime the HDG is at revision 2.6 and the datasheet at revision 3, and there is still the mentioned "contradiction" of 499R/1% vs. 500R/0.5%.

Consistency would be highly appreciated.

Thanks and Regards
Arne

0 Kudos
Reply