Hello,
I have an Embedded Linux distribution I created with Yocto running on XEN hypervisor on my iMX8QM MEK EVK board.
With this distribution, which is kernel 5.4.70, I want to get an image from my HDMI display over XEN.
Is this possible?
Can you support me on this issue?
Best regards,
Efecan
Hello,
Yes, it is possible, but you should change to the latest kernel, bus are fixed.
Regards
Hello,
Unfortunately I cannot update my Kernel version in my Yocto project.
With the dts included in the attachments, I was able to receive video from HDMI in my Embedded Linux distribution running on XEN.
But when I use this dts I cannot create DomU for my Android Automotive OS 10.
When I try to create a DomU I get the error "Device or resource busy".
What should I change in "imx8qm-mek-domu.dts" to create Android Automotive OS 10 DomU?
I'm fresher to this, can you help me?
Best regards,
Efecan