iMX8QM DDR Configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX8QM DDR Configuration

3,526 次查看
sbertrand
Contributor III

Hi,

I would like to understand how to configure DDR for iMX8QM system.

Our board has 8Go of DDR4 which is more than the iMX8QM MEK board.

How to configure the system to indicate additional RAM to initialize ?

How is the DDR configured ?

There are 2 channels, are they configured in interleaved mode ?

How the channel mapped to the memory region ?

The SCFW porting kit has a number of tests that can be run. Some are relevant to DDR.

I am able to run the DDR and DRC test on iMX8QM MEK but the DDR stress test fails :

*** DDR Stress SC Test

Power up DRC 0
Power up DRC 1
Allocate memory
Init DDRC
board_init_ddr(1)
DDR frequency = 1596000000
board_init_ddr(0)
DDR frequency = 1596000000
Current DDR Clock rate:
- DRC controller0: 798000000Hz, -DDR0 PHY: 1596000000Hz
- DRC controller1: 798000000Hz, -DDR1 PHY: 1596000000Hz
The DDR stress test can run with an incrementing frequency or at a static freq
To run at a static freq, simply set the start freq and end freq to the same value

Enter desired START freq in MHz and in 50MHz increments, then hit enter.

For example, for 1GHz, enter 1000, for 850MHz, enter 850.
1596
The freq you entered was: 1596 MHz

Enter desired END freq in MHz and in 50MHz increments, then hit enter.
Make sure this is equal to or greater than start freq
1596
The freq you entered was: 1596 MHz

Do you want to run DDR Stress Test for simple loop or infintely (till failure)?
Type '0' for simple loop. Type '1' for infinte test
0

----------------------------
DDR freq passed into function * 1000000: 1596000000

** pm_clock_enable error!, err 6
**Error occurred when trying to set DDR freq, re-start test

DDR Stress test ended due to detected data failure

Regards,
Stan

标记 (4)
3 回复数

3,021 次查看
vinothkumars
Senior Contributor IV

Hi @sbertrand ,

 

Will you please provide the steps to DDR Test Calibration and DDR value initialization for IMX8QM board.

Regards,
Vinothkumar Sekar
0 项奖励
回复

3,284 次查看
Stefan_ng
Contributor II

Hi Stan,

There exists a RPA Tool (RegisterProgrammingAid) for the DDR configuration (it's) an Excel Sheet. With this you can extract two files: *.cfg and *.ds.

With the ds you can run the NXP DDR Tool and with the cfg you have to build a new SCFW.

Pls. contact your NXP rep. for this files and tools.

This link might be useful, too: https://community.nxp.com/docs/DOC-341872 

BR,
Stefan

3,284 次查看
sbertrand
Contributor III

We got the RPA and the stress test tool.

The new configuration for 8Gbyte has been made. Testing will be performed soon.

Regards,
Stan