iMX8MQ got stuck during booting rootfs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8MQ got stuck during booting rootfs

1,559 Views
ida_jiang
Contributor III

Hi,

   I'm tring to use NFS to mount rootfs at iMX8MQEVK. The images used could boot from emmc normally. When I downloaded the image & dtb by DHCP and mounted the rootfs using NFS, the boot log showed that the board mounted successfully. But it was strange that the rootfs would get stuck as follows:1.png

   Dose anyone have idea about this problem?

   Thank you !

Labels (1)
Tags (1)
5 Replies

1,465 Views
ida_jiang
Contributor III

Hi igorpadykovkaran.gajjar@volansystech.com

I tried to mount a simplest rootfs made by myself and it succeeded.

So I think there are too many services that need to be started to cause this stuck.

Thanks & Best Regards

Ida

0 Kudos
Reply

1,465 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ida

one can try steps described in sect.4.7.5 Running the Linux image from NFS

attached Linux Guide with Demo Image

Linux Binary Demo Files - i.MX 8M Quad EVK

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,465 Views
ida_jiang
Contributor III

Hi igor ,

   Thank you for reply.

   I was working on this document before. The images were demo except the dtb.

   Because the board was made by ourselves according to the official design, and we could boot it from emmc or sd normally. What I changed at dts was " pcie0 disabled ".

   But when it used NFS, there would be this problem. Do you have any idea ?

Best Regards,

Ida

0 Kudos
Reply

1,465 Views
karangajjar
Senior Contributor II

Hi Ida J,

We are able to NFS boot the iMX8MQEVK using the below link:

Boot I.MX6q SABRE over the Network using TFTP and NFS  

You can use the binary image as suggested by Igor.

Regards,

Karan Gajjar

0 Kudos
Reply

1,465 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ida

 

for narrowing down issue (if this is caused by custom board)

recommended to try to reproduce issue on nxp reference board

with demo images.

 

Best regards
igor