iMX8MM ECSPI not probed in Kirkstone

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8MM ECSPI not probed in Kirkstone

Jump to solution
550 Views
dpog
Contributor IV

We recently moved from Yocto Dunfell to Kirkstone and switched the Kernel from 5.4 to 6.0 and 5.15 (we tried both approaches to solve this)

After doing so, the ECSPI is not probed any more in the Kernel boot. Did any changes occur, so that the device tree might not be parsed correctly, or did some Configurations change? 

The working DTS-part from 5.4 looks like this:

&ecspi1 {
    #address-cells = <1>;
    #size-cells = <0>;
    fsl,spi-num-chipselects = <1>;
    pinctrl-names = "default";
    pinctrl-0 = <&pinctrl_ecspi1 &pinctrl_ecspi1_cs>;
    cs-gpios = <&gpio5 9 GPIO_ACTIVE_LOW>;
    status = "okay";

    spidev0: spi@0 {
        reg = <0>;
        compatible = "linux,spidev";
        spi-max-frequency = <10000000>;
    };
};
 
pinctrl_ecspi1: ecspi1grp {
        fsl,pins = <
            MX8MM_IOMUXC_ECSPI1_SCLK_ECSPI1_SCLK    0x82
            MX8MM_IOMUXC_ECSPI1_MOSI_ECSPI1_MOSI    0x82
            MX8MM_IOMUXC_ECSPI1_MISO_ECSPI1_MISO    0x82
        >;
    };

    pinctrl_ecspi1_cs: ecspi1csgrp {
        fsl,pins = <
            MX8MM_IOMUXC_ECSPI1_SS0_GPIO5_IO9       0x82
        >;
    };
Labels (1)
0 Kudos
Reply
1 Solution
534 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @dpog,

I hope you are doing well.

This issue seems to be due to compatible string issue in spidev.

In the latest version of spidev.c driver support for the "spidev" compatible string is removed because of the below reason.

 
One can use any other compatible property from spidev_dt_ids[] table in drivers/spi/spidev.c
 
For example:
  spidev0spi@0 {
        reg = <0>;
        compatible = "rohm,dh2228fv";
        spi-max-frequency = <10000000>;
    };
 
 
Thanks & Regards,
Dhruvit Vasavada

View solution in original post

0 Kudos
Reply
1 Reply
535 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @dpog,

I hope you are doing well.

This issue seems to be due to compatible string issue in spidev.

In the latest version of spidev.c driver support for the "spidev" compatible string is removed because of the below reason.

 
One can use any other compatible property from spidev_dt_ids[] table in drivers/spi/spidev.c
 
For example:
  spidev0spi@0 {
        reg = <0>;
        compatible = "rohm,dh2228fv";
        spi-max-frequency = <10000000>;
    };
 
 
Thanks & Regards,
Dhruvit Vasavada
0 Kudos
Reply