iMX8M two qspi issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX8M two qspi issue

1,453件の閲覧回数
weikeng-jimmy
Contributor III

Hi Sir,

Customer want to enable two chip (w25q64dw) , but QSPI_B always probe failed as beolw message.

# dmesg | grep -i spi
[ 2.084054] fsl-quadspi 30bb0000.qspi: w25q64dw (8192 Kbytes)
[ 2.091144] fsl-quadspi 30bb0000.qspi: unrecognized JEDEC id bytes: ff, ff, ff
[ 2.098393] fsl-quadspi 30bb0000.qspi: Freescale QuadSPI probe failed
[ 2.104945] fsl-quadspi: probe of 30bb0000.qspi failed with error -2

I.MX8M only support two planes in one die mode ?

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 返信

1,319件の閲覧回数
art
NXP Employee
NXP Employee

Is the IOMUX configured correctly for the QSPI_B channel signals? Can you see any activity on the QSPI_B channel signals when trying to access it? Please check.

0 件の賞賛
返信