iMX8M mini evk+MIPI to HDMI
OS : Yocto 2.5
Kernel : 4.14.98-2.0.1
DSI to HDMI CHIP: ADV7535
HDMI hot plug issue
1. HDMI hot plug screen freezes , but use uart port confirm system normal
2. HDMI hot plug screen and system normal , but wayland terminal windows disappear
The probability of issue one is 70%
The probability of issue two is 30%
Hi Diego,
Our customized board is based on iMX8MQ-EVK. Display and system work well with HDMI hotplug. But, Wayland/Weston Terminal is gone when HDMI cable unplugged/re-plugged in, which is very weird...
Do you know how to solve this issue? The following are contents of " /etc/xdg/weston/weston.ini"
[core]
gbm-format=argb8888
idle-time=0
#use-g2d=1
xwayland=true
[shell]
size=1920x1080
[libinput]
touchscreen_calibrator=true
#[output]
#name=HDMI-A-1
#mode=1920x1080@60
#transform=90
#[output]
#name=HDMI-A-2
#mode=off
# WIDTHxHEIGHT Resolution size width and height in pixels
# off Disables the output
# preferred Uses the preferred mode
# current Uses the current crt controller mode
#transform=90
[screen-share]
command=/usr/bin/weston --backend=rdp-backend.so --shell=fullscreen-shell.so --n
thanks,
Jason
Hello,
There was not a problem with the driver. The problem was on the device tree.
To solve the problem you need to add the below interrupt on the device tree.
adv7535@3d {
compatible = "adi,adv7535";
reg = <0x3d>;
adi,addr-cec = <0x3b>;
adi,dsi-lanes = <0x4>;
+ pinctrl-0 = <0x55>;
+ interrupt-parent = <0x55>
+ interrupts = <0x7 0x8>;
status = "okay";
port {
endpoint {
remote-endpoint = <0x23>;
linux,phandle = <0x50>;
phadle = <0x50>
};
};
};
Whit that configuration the hot-plug should work.
Best regards,
Diego.