iMX7 S/D Registers file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX7 S/D Registers file

757 Views
francoislion
Contributor I

Hello,

I am currently evaluating the iMx7 processor using a Mx7D sabre board and DS-5.

It is a bare metal project so I need peripheral register files, and I have found them on your web site: (Header_Files_Include_for_i.MX__Pins_Tool_1.0.zip)

Using them I had really weird problems and I finally found that the origin of my problems are the description file itself (iMX7D_registers.h). In my case the CCM module description is totally wrong, maybe other modules are also wrong...

Do you plan to fix them and when ?

Kind regards,

François Lion

Labels (2)
0 Kudos
Reply
2 Replies

633 Views
francoislion
Contributor I

Thank you Joan, but I know this tool, and the header files I used have been designed to work with:

http://cache.nxp.com/files/soft_dev_tools/software/app_software/application_development_framework/He... 

However, I  noticed that the web site displays (REV 1.1) while the file is Header_Files_Include_for_i.MX__Pins_Tool_1.0.zip.

And the problem of the file is not a pin muxing problem but some peripheral registers are not mapped to the right address. For example in the CCR structure definition, companion registers (SET, CLR & TGL) are missing, and that creates a shift in the following register addresses...

0 Kudos
Reply

633 Views
joanxie
NXP TechSupport
NXP TechSupport

one can try new pin tools, I send the guide document to you for reference, and one can give comment for that

https://community.nxp.com/docs/DOC-331984?commentID=36965#comment-36965 

0 Kudos
Reply