iMX6q Turn Off LVDS and HDMI on boot up

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6q Turn Off LVDS and HDMI on boot up

909件の閲覧回数
ritesh_panchal
Contributor I

I am using im6qsabresd board. I am using x11 fsl-image-gui image.

I want to disable LVDS and HDMI output on booting. Just enabling UART console. And i just want to on LVDS or HDMI when i execute video play command. And after completion of video, turn off the LVDS and HDMI video.

I found that on boot up setting u-boot environment parameter will turn off LVDS/HDMI. But i unable to turn off. Can you show procedure for doing this?

I can able to turn off or on LVDS display after boot up by using following commands.

xset -display :0.0 dpms force off

xset -display :0.0 dpms force on

But can i make on/off display in gstreamer or gplay command?

ラベル(5)
0 件の賞賛
返信
2 返答(返信)

627件の閲覧回数
b36401
NXP Employee
NXP Employee

You can make a plugin for gstreamer that serves the functionality you need (turn off/on the display).

Have a great day,                                                                                                                                                                  

Victor                                                                                                                                                                             

                                                                                                                                                                                   

-----------------------------------------------------------------------------------------------------------------------                                                            

Note: If this post answers your question, please click the Correct Answer button. Thank you!                                                                                       

-----------------------------------------------------------------------------------------------------------------------                                                            

0 件の賞賛
返信

628件の閲覧回数
vijaikumar
Contributor III

For all the framebuffers you want to disable, you can use video= parameter

video=mxcfb0:off video=mxcfb1:off video=mxcfb2:off

0 件の賞賛
返信