iMX6ULL can't connect to WiFi if band-steering is enabled ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6ULL can't connect to WiFi if band-steering is enabled ?

513 Views
kevinw25
Contributor I

We're using the iMX6ULL and the LBEE5KL1DX WiFi/Bluetooth module. We are experiencing a problem where our device times out anytime it tries to connect to a Wi-Fi network with bandsteering enabled - it tries to connect but is never able to. When connecting to a 2.4 GHz network, there is no problem. 

I'm not clear on where this problem would be located - would it be in the kernel config ? Or does something specific have to be included in the application layer code.

As far as I could tell, it is the LBEE5KL1DX that should handle this automatically since the transceiver hardware ONLY supports 2.4 GHz. Any help is much appreciated ! 

0 Kudos
Reply
1 Reply

479 Views
jimmychan
NXP TechSupport
NXP TechSupport

It maybe the driver or firmware problem. You may need to ask the module provider to support this issue.

0 Kudos
Reply