iMX6UL fast RTS inactivation in RS-485 mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX6UL fast RTS inactivation in RS-485 mode

1,226 次查看
konstantinyatse
Contributor I

Dear, RIOT

I need your help or some advice in the following problem:

        

Input information:

                I work with i.MX 6UltraLite EVK – development board for iMX6ul processor.

                Prepared Linux image based on Buildroot and configured by defconfig for this board.

                Linux kernel version : v4.9.11 (from official freescale git repo).

My goal is realization of UART in RS485 mode with RTS inactivation time no higher than 20us after TX is finished.  

At now, driver has deactivation time for about 20 ms after TX is finished.

 

I test this at simply program:

         open file descriptor to tty

         use send POSIX [write] gunction to send data

         close file descriptor

 

Current version of driver I am working on : http://elixir.free-electrons.com/linux/v4.9.11/source/drivers/tty/serial/imx.c

 

I have realized that this driver is for several types of processors of one family with similar register map, but I haven’t found in code any particular comments on specific realization, except some comments in probe function.

 

How to modify the driver code for fast (as much as could be possible) inactivation RTS gpio after TX is finished.

 

Thank, you for help.

标签 (1)
0 项奖励
1 回复

563 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Konstantin

please look on

[imx6] RS485 could be supported on Imx6 series ?  

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励