Hello,
I am using an iMX6UL evk in combination with a µC module. The µC is connected to the iMX's UART2 (ttymxc1, since I'm using the default dt configuration provided for the 14x14 evk). The evk is running a Yocto Linux image with kernel 4.1.15.
My application requires the iMX6 to be in the lower possible power state for most of the time, so I've configured it to enter DSM mode (using "echo mem > /sys/power/state") and wake up on interrupts from the UART pins, so that whenever the µC module has any data to transmit, the iMX can wake up and handle the coming messages. Wake up on UART is configured echoing "enabled" into the corresponding sysfs "wakeup" entry.
What I'm currently achieving is:
My questions are then the following:
Thank you for your help
Giorgio
Hi Giorgio
first character could be lost as mentioned in sect.53.8.2 UART Operation
in System Stop Mode i.MX6UL Reference Manual
http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6ULRM.pdf
When an asynchronous WAKE (awake) interrupt exits the ARM platform from STOP
mode, make sure that a dummy character is sent first because the first character may not
be received correctly.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
thank you very much for your reply.
The manual says that I should lose a character, but experimentally I'm noticing a different behavior using the 4.1.15 kernel and the provided yocto image.
I'm testing such behavior setting up the serial port (@155200 bps) and issuing a "cat /dev/ttymxc1" command, since the external µC module is sending out ascii chars (i'm testing it sending periodically the "1234567890abcdefghijklmnopqrstuvwxyz" string).
If the iMX EVK is in RUN mode everything works as expected, the message is correctly shown in the console.
If i put the iMX in STOP mode (issuing the "echo mem > /sys/power/state" command) it wakes up correctly as soon as the µC transmits the message, but the string printed out by the cat command is something like "tuvwxyz", so i'm losing much more than a single char.
It looks like some data is lost before the system is woken up. Could it be a driver or configuration related issue?
How can I further investigate the issue? Do you have any debugging hint?
Best Regards,
Giorgio