iMX6S ADMA interrupt - timeout

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6S ADMA interrupt - timeout

1,064件の閲覧回数
philippeleduc
Contributor II

Hello,

I managed to configure the ADMA2 of the iMX6S uSDHC module. I can read and write the SD card with it. However, the DMA interrupt is never set (DINT in  uSDHC_INT_STATUS) while the Transfer COmplete bit is set.

Here is a dump of the registers after a successfull read operation:

=======================uSDHC0 dump===================

DS_ADDR:               0x1459be00

BLK_ATT:               0x00000200

CMD_ARG:             0x07400000

CMD_XFR_TYP:    0x123a0000

CMD_RSP0:             0x00000900

CMD_RSP1:             0xb9edb7ff

CMD_RSP2:             0x325b5983

CMD_RSP3:            0x00000b00

DATA_BUFF_ACC_PORT: 0x00000000

PRES_STATE:          0xff8d8088

PROT_CTRL:           0x00800222

SYS_CTRL:               0x008e013f

INT_STATUS:          0x00000003

INT_STATUS_EN:   0x157f513f

INT_SIGNAL_EN:    0x1070000a

AUTOCMD12_ERR_STATUS: 0x00000000

HOST_CTRL_CAP:  0x07f30000

WTMK_LVL:            0x08000880

MIX_CTRL:              0x00000037

FORCE_EVENT:       0x00000000

ADMA_ERR_STATUS: 0x00000000

ADMA_SYS_ADDR:  0x153dd008

DLL_CTRL:               0x00000000

DLL_STATUS:          0x00000200

CLK_TUNE_CTRL_STATUS: 0x00000000

VEND_SPEC:            0x20007809

MMC_BOOT:          0x00000000

VEND_SPEC2:          0x00000006

As you can see, the TC bit and the CC bit are set, but the DINT is not. However every IT bits are set in the STATUS_EN register.

Does someone know where I am going wrong?

Thank you i advance,

Regards,

ラベル(6)
0 件の賞賛
返信
5 返答(返信)

850件の閲覧回数
philippeleduc
Contributor II

Well, it is a proprietary RTOS so I am not allowed to share this fix (which shouldn't be meaningful for another OS).

0 件の賞賛
返信

850件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

Ok, got it.

0 件の賞賛
返信

850件の閲覧回数
philippeleduc
Contributor II

I finally identified the problem of the ADMA setup: there was a bug in the cache management function --> the BD structure was not flushes correctly. I have also check the ERR004364 but it seems that there is not concerns with it (thank you anyway Yuri :smileyhappy:).

0 件の賞賛
返信

850件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

Which OS are you using? Care to share the fix?

0 件の賞賛
返信

850件の閲覧回数
Yuri
NXP Employee
NXP Employee

   Please try to apply the workaround for the next item from the Errata :

ERR004364 uSDHC: Limitations on uSDHC3 and uSDHC4 clock-gating

Workarounds:

uSDHC3 and uSDHC4 clock-gating controls should not be configured to gate the clocks in case

RAWNAND and APBADMA are used. There are two registers in CCM that need to be configured

accordingly:

• CCGR: Gating of the clock according to power mode

• CMEOR: Enable/Disable dynamic clock gating

http://cache.freescale.com/files/32bit/doc/errata/IMX6DQCE.pdf

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信