iMX6Q is too hot about 85 C

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6Q is too hot about 85 C

788 Views
tamilarasane
Contributor III

Hi all,

we designed Custom SOM using imx6q processor  by following saber design files

when subway surf game (android game app, requires 1Ghz speed) is loaded,  imx6q die temperature reaches 85 C within 15 min.

It is reduced to 40 C immediately after closing this game app.

we also used heat sink,in this case  it is around 76 C (10 hrs continuous test under ambient temperature 22 C).

let me know how to reduce the die temperature when processor runs at its maximum frequency of 1 Ghz/1.2Ghz

both in software and hardware ?

r anyone faced this much die temperature..? is it normal..?

Thanks,

Tamilarasan

0 Kudos
Reply
2 Replies

483 Views
igorpadykov
NXP Employee
NXP Employee

Hi Tamilarasan

please look at appnotes below it gives suggestions for thermal

management

AN4579 i.MX 6 Series Thermal Management Guidelines

AN4509 i.MX 6Dual/6Quad Power Consumption Measurement

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

483 Views
saurabh206
Senior Contributor III

Hi

Have you try to run subway surf game on SabreSDB or other Freescale hardware?

This will provide useful information.

Thanks

Saurabh

0 Kudos
Reply