iMX6Q+SGTL5000 have pop noise in suspend/resume and shutdown processes

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6Q+SGTL5000 have pop noise in suspend/resume and shutdown processes

1,048 Views
bakbad
Contributor III

Hello, NXP

I have a custom board with imx6q and sgtl5000, but when the machine get into suspend or wake up or shutdown, the speaker had a "pop" noise. I had tried this: setting the DAC_MUTE_LEFT and DAC_MUTE_RIGHT bit in suspend function, and clear them in resume function, but it didn't works. Any advices? Thanks.

Best Regards,

bo xu

Labels (3)
0 Kudos
3 Replies

871 Views
bakbad
Contributor III

Hello, everyone

I  solved this problem by closing the amplifier(TS4962)'s STBY pin before the system get into suspend, for letting the machine get into suspend we use commands like this "echo 'mem' > /sys/power/state" in the application layer.

The processes just like this:

echo 0 > /sys/class/gpio/gpio204/value (num 204 is the pin number of TS4962's STBY, before get into suspend)

echo "mem" > /sys/power/state (getting into suspend)

echo 1 > /sys/class/gpio/gpio204/value (in wakeup process)

And the pop-click noise has gone.

0 Kudos

871 Views
igorpadykov
NXP Employee
NXP Employee

Hi bo

additionally one can consider decreasing volume as described in

sect.2.2.6 Volume Control AN3663 SGTL5000 Initialization and Programming

http://cache.freescale.com/files/analog/doc/app_note/AN3663.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

871 Views
bakbad
Contributor III

Hi igorpadykov,

Thanks for  your advice.I tried as section 2.2.6 told.but when i put the code in sgtl5000_suspend() like this:

static int sgtl5000_suspend(struct snd_soc_codec *codec)

{

   

   // Configure ADC left and right analog volume to desired default.

   snd_soc_write(codec, SGTL5000_CHIP_ANA_ADC_CTRL, 0x0000);

   // LINEOUT and DAC volume control

   snd_soc_update_bits(codec, SGTL5000_CHIP_ANA_CTRL, 8, 0);

   snd_soc_write(codec, SGTL5000_CHIP_DAC_VOL, 0x3c3c);

   snd_soc_update_bits(codec, SGTL5000_CHIP_ADCDAC_CTRL, 2, 0);

   snd_soc_update_bits(codec, SGTL5000_CHIP_ADCDAC_CTRL, 3, 0);

   // Unmute ADC

   snd_soc_update_bits(code, SGTL5000_CHIP_ANA_CTRL, 0, 0);

   sgtl5000_set_bias_level(codec, SND_SOC_BIAS_OFF);

   return 0;

}

and rebuild the kernel for the machine. But the machine had no sound before i set it to suspend and when the machine got into suspend status, it can't wake up.Did i missed something?

Best Regards,

bo xu

0 Kudos