iMX6Q Android 9 custom board Ethernet ip address not assigned

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6Q Android 9 custom board Ethernet ip address not assigned

856件の閲覧回数
Aravinthkumar
Contributor III

Hi Team,

I'm using iMX6q custom board with Android 9. we have done the required modification for ethernet and boot-up interface is up. we can see the log. But IP address not assigned and we can't browse it.

 


sabresd_6dq:/ $ fec 2188000.ethernet eth0: Link is Up - 100Mbps/Full - flow control off
IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready

sabresd_6dq:/ $

 

sabresd_6dq:/ # ifconfig
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
inet6 addr: ::1/128 Scope: Host
UP LOOPBACK RUNNING MTU:65536 Metric:1
RX packets:16 errors:0 dropped:0 overruns:0 frame:0
TX packets:16 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:1152 TX bytes:1152

eth0 Link encap:Ethernet HWaddr 00:aa:bb:cc:dd:ee Driver fec
inet6 addr: fe80::f9a1:6779:71dd:4ddf/64 Scope: Link
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:27 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 TX bytes:4182

 

 

sabresd_6dq:/ # logcat
--------- beginning of main
06-24 07:48:13.268 235 340 E display : threadLoop invalid uevent change@/devices/soc0/pwm-backlight/backlight/pwm-backlight
fec 2188000.ethernet eth0: Link is Up - 100Mbps/Full - flow control off
06-24 07:48:16.812 423 444 I EthernetTracker: interfaceLinkStateChanged, iface: eth0, up: true
06-24 07:48:16.813 423 531 D EthernetNetworkFactory: updateInterfaceLinkState, iface: eth0, up: true
06-24 07:48:16.813 423 531 D EthernetNetworkFactory: starting IpClient(eth0): mNetworkInfo=[type: Ethernet[], state: DISCONNECTED/IDLE, reason: (unspecified), extra: (none), failover: false, available: false, roaming: false]
06-24 07:48:16.820 217 261 D CommandListener: Clearing all IP addresses on eth0
06-24 07:48:16.877 423 1553 D DhcpClient: Receive thread started
06-24 07:48:16.882 423 1552 D DhcpClient: Broadcasting DHCPDISCOVER

0 件の賞賛
返信
1 返信

847件の閲覧回数
Aravinthkumar
Contributor III

Issue fixed. 

 

Thanks.

0 件の賞賛
返信