iMX6DL : Is the USB_OTG_ID pin necessary for USB boot (Serial Downloader) ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6DL : Is the USB_OTG_ID pin necessary for USB boot (Serial Downloader) ?

1,442件の閲覧回数
koichisakagami
Contributor II

Dear community,

I consider using the Serial Downloader .
Please see Table 89 (p.133) in IMX6SDLIEC (Rev.3).


The allocated pads during boot for USB interface are USB_OTG_DP , USB_OTG_DN and USB_OTG_VBUS.
There is not USB_OTG_ID pin.

Is the USB_OTG_ID pin necessary for USB boot (Serial Downloader) ?

Best Regards,
Koichi Sakagami

ラベル(1)
1 返信

684件の閲覧回数
Yuri
NXP Employee
NXP Employee

  To be fully on safe side it may be recommended to follow USB standards and terminate

all associated signals properly. In the same time, looks like, no additional pins configured / used
(except USB_OTG_DN / DP) by the  boot ROM in Serial (USB) boot mode. I checked it on my SDP.

All related signals / pins (USB_OTG_ID, USB_OTG_OC, USB_OTG_PWR) are configured in default
(after reset) state, when IOMUXC_SW_MUX_CTL_PAD_xxx[MUX_MODE] = 5 (GPIO).


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信