iMX6DL : DDR3 CLK successive output

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMX6DL : DDR3 CLK successive output

跳至解决方案
703 次查看
koichisakagami
Contributor II

Dear community,

We investigate a DDR3 clock quality for JEDEC clock jitter test.
We need to output the DDR3 clock continuously .

We executed the " mtest command " on uboot.
However the clock became the intermittent output.

Question.
What kind of method can we output the DDR3 clock in continuously ?

Best Regards,
Koichi Sakagami

0 项奖励
1 解答
492 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  The i.MX6 MMDC provides clock for DRAM parts, and  - I am afraid -

this is impossible to configure clock generation logic in order to get
continuous  or burst clocks. Basically, clocks are started as soon as

a DRAM chip select is enabled.

  Please try using Stress DDR tool.

https://community.freescale.com/docs/DOC-96412

https://community.freescale.com/docs/DOC-105652


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
1 回复
493 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  The i.MX6 MMDC provides clock for DRAM parts, and  - I am afraid -

this is impossible to configure clock generation logic in order to get
continuous  or burst clocks. Basically, clocks are started as soon as

a DRAM chip select is enabled.

  Please try using Stress DDR tool.

https://community.freescale.com/docs/DOC-96412

https://community.freescale.com/docs/DOC-105652


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励