We have a custom board and a Variscite DART-MX6, both equipped with the Micrel KSZ9031 Gigabit Ethernet Tranceiver. On both I have the same issue.
When hitting suspend, the LEDs do not turn off, but light up constantly at a dimmed down level. If the ethernet cable is not connected and the lights are off when I invoke suspend, it still decides to light up again.
I've looked at the Micrel datasheet, as well as the linux drivers for fec/micrel, but find nothing to "defend" this kind of behaviour, so I just wanted to say it out loud here in case someone has a clue.
Figured this one out. It is not VGEN5, but 2P5 that disappears in suspend.
From arch/arm/mach-imx/anatop.c
if ((imx_mmdc_get_ddr_type() == IMX_DDR_TYPE_LPDDR2) &&
!imx_gpc_usb_wakeup_enabled())
imx_anatop_enable_2p5_pulldown(true);
else
imx_anatop_enable_weak2p5(true);
A relevant commit message:
Since i.MX6SX, if USB vbus wake up is enabled, weak 2P5
needs to be on even if the DRAM is LPDDR2, previously, we need
to set stop_mode_config to keep 2P5 on, so enter DSM,
if USB vbus wakeup is enabled, we need to keep weak 2P5 on.
Leaving weak 2P5 on fixes my issue.
Hi Anders
led behaviour is defined by "LED Mode" described in KSZ9031 datasheet Table 9,10
(configured LED_MODE strap-in (Pin 41)). Additionally one can change behaviour
in driver, described in Chapter 43 Fast Ethernet Controller (FEC) Driver
attached Linux Manual.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks. I've read both of those before, without finding anything that can explain the behaviour. I forgot to mention that I've tried compiling a kernel with fec and micrel as modules. If I remove the modules the LEDs go out, but if I suspend they come back on in a dimmed state.
I think this happens because on vgen5 drops from 2.5V to 1.33V in sleep, so the pull-up is not strong enough to turn off the leds. Need to find out why and how to prevent it...
EDIT: that, or the 2.5V is disabled completely in suspend.