iMX6 Solox UART

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6 Solox UART

748件の閲覧回数
vinythambi
Contributor I

In iMX6 SoloX development board design(SPF-27962), UART1 and UART2 are dedicated for A9 and M4 respectively. Does these pins have to be maintained for custom boards design or debug UART can be changed to any of the other UARTs available?

ラベル(1)
0 件の賞賛
返信
1 返信

675件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi,
Debug UARTs could be changed, but it is required to consider all the proper settings. Please refer to the following Community threads for details:
imx6 debug uart change 
Change debug UART 
imx6q change uboot debug uart 1 to uart 2 

The main issue of not having externally available the UART1 could be in case of requiring the Serial Downloader Mode by UART instead of by USB, because the serial downloader UART cannot be changed on the ROM code.

Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

0 件の賞賛
返信