Hi,
We are using imx6Q sabresd platform for our development with Linux 3.14.28_1.0.0-GA BSP.
From the below board file we could see the following function "setup_pmic_voltages".
~/u-boot-imx/board/freescale/mx6sabresd/mx6sabresd.c
We understood that, after detection of PMIC
1. VGEN3 and VGEN5 voltages are increased to 2.8v and 3.0v respectively.
2. The SW1AB and SW1C standby voltages are set to 0.975v.
We would like to know, why the SW1AB and SW1C standby voltages are set to 0.975? and where this voltage will be used?
Regards,
Ansari
Hi Abdul
uboot does not use low power modes, they are used in linux,
please refer to Chapter 22-25 attached Linux Manual from L3.14.28_1.0.0_iMX6QDLS_BUNDLE
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear Igor,
Thank you for your input in our request.
We believe, the SW1AB and SW1C standby registers(0x21 & 0x2F respectively) are not accessed in the below driver file.
~/linux-imx/drivers/regulator/pfuze100-regulator.c
Please let us know, in Linux kernel where the SW1AB and SW1C standby voltages used during the low power mode.
From the PFUZE100 data sheet, we understood as below
When the PMIC enters into standby mode(CPU request for standby mode), the regulator(SW1AB & SW1C) will use the set point as programmed by SW1xSTBY[5:0]. Is this correct?
Please correct us if we are wrong.
Regards,
Ansari
Hi Abdul
Linux Manual shows used files.
>When the PMIC enters into standby mode(CPU request for standby mode), the regulator
>(SW1AB & SW1C) will use the set point as programmed by SW1xSTBY[5:0]. Is this correct?
yes.
Best regards
igor
Dear Igor,
Thanks for your input.
>>When the PMIC enters into standby mode(CPU request for standby mode), the regulator
>>(SW1AB & SW1C) will use the set point as programmed by SW1xSTBY[5:0]. Is this correct?
>yes.
We believe, the SW1xSTBY[5:0] register values are not modified or updated in the Linux level and the standby set point values are maintained for 0.975v(which is set in u-boot level).
Please let us know, in Linux kernel where the SW1AB and SW1C standby voltages used during the low power mode or it is not required to update the SW1xSTBY register values.?
Please correct us, if we are wrong.
Regards,
Ansari