iMX6 L2 cache size different between iMX6SDL and iMX6DQ variants?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 L2 cache size different between iMX6SDL and iMX6DQ variants?

Jump to solution
2,184 Views
MichaelV
Senior Contributor II

The RM's for the SDL and DQ state in chapter 12.3.3 that the size of the L2 cache of the DQ is 1 MB and that of the SDL is 512 KB, but as comment it states: "Size is implied by the Cache-Size times cache-ways".

However, both SDL and DQ RMs tables state 64 KB for cache way size and both state they have 16 ways. This would mean both SDL and DQ have 64 * 16 = 1MB of L2 cache.

Table 12-5 is contradicting itself. Which row is containing the wrong information?

Chapter 1.4 "Features" also states the SDL and DQ L2 cache sizes are different. However, the text in this chapter is also contradictory... The SDL RM first states "512 KB unified I/D L2 cache", but a couple of lines lower (under the heading "The memory system consists...") it states "Level 2 Cache—Unified instruction and data (256 KB)" (whereas the DQ RM has 1MB in both locations of chapter 1.4).

So, does the SDL have 1 MB (determined from 1st two rows of table 12-5), 512 KB (last row of table 12-5 and beginning of section 1.4) or 256 KB (couple of lines lower in section 1.4)?

Best guess is that the SDL has 8 ways of 64 KB cache, but maybe this is 16 ways of 32 KB cache?

Would be great to get that cleared up, thanks.

Labels (4)
Tags (3)
1 Solution
1,131 Views
igorpadykov
NXP Employee
NXP Employee

Hi Michel

SDL has 512 KB L2 size.

Actually running Linux one can see logs reading L2 Auxiliary Control Register,

for example fom link below:

"L310 cache controller enabled

l2x0: 16 ways, CACHE_ID 0x410000c8, AUX_CTRL 0x02050000, Cache size: 524288 B"


Linux Kernel stuck while booting at "i.MXC CPU frequency driver"

AUX_CTRL 0x02050000  means 16 ways of 32 KB

ARM Information Center

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,132 Views
igorpadykov
NXP Employee
NXP Employee

Hi Michel

SDL has 512 KB L2 size.

Actually running Linux one can see logs reading L2 Auxiliary Control Register,

for example fom link below:

"L310 cache controller enabled

l2x0: 16 ways, CACHE_ID 0x410000c8, AUX_CTRL 0x02050000, Cache size: 524288 B"


Linux Kernel stuck while booting at "i.MXC CPU frequency driver"

AUX_CTRL 0x02050000  means 16 ways of 32 KB

ARM Information Center

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,131 Views
MichaelV
Senior Contributor II

Thanks!

To recap:

iMX6DQ has 16 ways of 64 KB = 1024 KB of L2 cache

iMX6SDL has 16 ways of 32 KB = 512 KB of L2 cache

PS. Not everybody runs Linux... :smileywink: