iMX6 DualLite and iMX6 Solo Processor Pin-outs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 DualLite and iMX6 Solo Processor Pin-outs

868 Views
srinivasukimuru
Contributor I

Whether the IMX6 DualLite processor MCIMX6U7CVM08AC and iMX6

SOLO processor MCIMX6S7CVM08AC are same package, footprint and same pin-list. We want to use both the processors in a single prototype board for Software requirements proof of concept.

Labels (2)
0 Kudos
1 Reply

588 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi,

The i.MX6 DualLite and Solo shares practically all, including the datasheet:

http://www.nxp.com/assets/documents/data/en/data-sheets/IMX6SDLIEC.pdf

Therefore, you could design the hardware and software for any of the two and it should work in both, just considering the performance difference due to the missing core on the Solo.


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos