Hi,
For accessing max98088 driver, i try to update my iMX53 QSB from a linux 2.6.35.3 to a linux 2.6.38.
To do it I've changed my setting in ltib to use a 2.6.38 linux. I update the source by downloading the last release (12.01.01).
It compiled successfully but, at runtime, I lose my serial console (UART 1) after "Uncompressing kernel... done, booting the kernel.".
To upload the new rootfs and uImage, I use MfgTool with the same config as before (I just changed rootfs.tar.bz2 and uImage).
Cordially
Cyril CROCQUESEL
解決済! 解決策の投稿を見る。
Hi,
I find the solution :
IMX serial support was not selected in kernel option
also console on IMX serial port
Now I have an other problem but this one is solve.
Thanks
Cyril
I've made a mistake, the uImage was not the good one.
No I get the next error : bad command from bootm. And I arrived on a prompt : "MX53-LOCO-BIN>"
I will make some test tomorrow And give the result
Cordially
Cyril
Updated at 04/04/2013 9:36 (GMT+1) :
Hi,
I success to boot the kernel with the following command :
MX53-LOCO U-Boot > setenv bootargs_base 'setenv bootargs console=ttymxc0,115200'
MX53-LOCO U-Boot > setenv bootargs_mmc 'setenv bootargs ${bootargs} root=/dev/mmcblk0p1 rootwait rw video=mxcdi1fb:GBR24,VGA-XGA di1_primary vga'
MX53-LOCO U-Boot > setenv bootcmd_mmc 'run bootargs_base bootargs_mmc;mmc dev 0;mmc read ${loadaddr} 0x800 0x1800;bootm'
MX53-LOCO U-Boot > setenv bootcmd 'run bootcmd_mmc'
MX53-LOCO U-Boot > saveenv
MX53-LOCO U-Boot > run bootcmd
But I have again no more information in the serial console after this message :
"Uncompressing kernel... done, booting the kernel."
The kernel start, at least, until the VGA start-up. (I can display the linux logo on the screen).
Cordially,
Cyril
Hi Cyril,
do you have enabled kernel output? Maybe your kernel is on a quiet boot. You can change the settings by modifying "menuconfig -> kernel hacking"
Cheers
MaTT
Hi,
I add in kernel option for kernel low level debug and also early printk. But this doesn't change the behavior at boot.
Would you like I join my .config file?
Cordially
Cyril
Hi,
I find the solution :
IMX serial support was not selected in kernel option
also console on IMX serial port
Now I have an other problem but this one is solve.
Thanks
Cyril