Hello Everybody,
We're developing an ethernet gateway device with the iMX283 processor.
Our problem is, that our NAND Flash has 1.8V levels, but the iMX is working with 3.3V levels over the GPMI Port.
We have set up the HW_PINCTRL_DRIVEx Register correctly for operations with 1.8V. The levels are now for about 250ns at 1.8 and then rise to 3.3V...
Our thought is, that something in the .dts file isn't set up correctly. Our .dts file looks currently like this:
/dts-v1/;
#include "imx28.dtsi"
#include <dt-bindings/gpio/gpio.h>
/ {
model = "IMX28 Modul";
compatible = "tem,imx28", "fsl,imx28";
memory {
reg = <0x40000000 0x08000000>;
};
};
&pinctrl {
pinctrl-names = "default";
pinctrl-0 = <&hog_pins_a>;
hog_pins_a: hog@0 {
reg = <0>;
fsl,pinmux-ids = <
/* RS485 Setup */
/* MX28_PAD_SAIF0_LRCLK__GPIO_3_21 */
MX28_PAD_SAIF0_LRCLK__AUART4_RTS
MX28_PAD_SAIF0_BITCLK__GPIO_3_22
MX28_PAD_SAIF0_BITCLK__AUART4_RX
/* MX28_PAD_SSP2_SS0__GPIO_2_19 */
MX28_PAD_SSP2_SS1__GPIO_2_20
MX28_PAD_SSP2_SS2__GPIO_2_21
>;
fsl,drive-strength = <MXS_DRIVE_4mA>;
fsl,voltage = <MXS_VOLTAGE_HIGH>;
fsl,pull-up = <MXS_PULL_DISABLE>;
};
gpmi_pins_b: gpmi-nand@0 {
reg = <0>;
fsl,pinmux-ids = <
MX28_PAD_GPMI_D00__GPMI_D0
MX28_PAD_GPMI_D01__GPMI_D1
MX28_PAD_GPMI_D02__GPMI_D2
MX28_PAD_GPMI_D03__GPMI_D3
MX28_PAD_GPMI_D04__GPMI_D4
MX28_PAD_GPMI_D05__GPMI_D5
MX28_PAD_GPMI_D06__GPMI_D6
MX28_PAD_GPMI_D07__GPMI_D7
MX28_PAD_GPMI_CE0N__GPMI_CE0N
MX28_PAD_GPMI_RDY0__GPMI_READY0
MX28_PAD_GPMI_RDN__GPMI_RDN
MX28_PAD_GPMI_WRN__GPMI_WRN
MX28_PAD_GPMI_ALE__GPMI_ALE
MX28_PAD_GPMI_CLE__GPMI_CLE
MX28_PAD_GPMI_RESETN__GPMI_RESETN
>;
fsl,drive-strength = <MXS_DRIVE_4mA>;
fsl,voltage = <MXS_VOLTAGE_LOW>;
fsl,pull-up = <MXS_PULL_DISABLE>;
};
};
&gpmi {
pinctrl-0 = <&gpmi_pins_b &gpmi_status_cfg>;
nand-on-flash-bbt;
status = "okay";
partition@0 {
label = "boot";
reg = <0x00000000 0x00300000>;
read-only;
};
partition@1 {
label = "environment";
reg = <0x00300000 0x00080000>;
};
partition@2 {
label = "redundant-environment";
reg = <0x00380000 0x00080000>;
};
partition@3 {
label = "kernel";
reg = <0x00400000 0x00400000>;
};
partition@4 {
label = "filesystem";
reg = <0x00800000 0x0f800000>;
};
};
&digctl {
status = "okay";
};
/* 1st TX-Std UART - (D)UART */
&duart {
pinctrl-names = "default";
pinctrl-0 = <&duart_4pins_a>;
status = "okay";
};
&mac0 {
phy-mode = "rmii";
pinctrl-names = "default";
pinctrl-0 = <&mac0_pins_a>;
status = "okay";
};
&mxs_rtc {
status = "okay";
};
&ocotp {
status = "okay";
};
&ssp0 {
compatible = "fsl,imx28-mmc";
pinctrl-names = "default";
pinctrl-0 = <&mmc0_4bit_pins_a>;
bus-width = <4>;
status = "okay";
};
&ssp2 {
compatible = "fsl,imx28-spi";
pinctrl-names = "default";
pinctrl-0 = <&spi2_pins_a>;
clock-frequency = <57600000>;
status = "okay";
cs-gpios = <&gpio2 19 0 &gpio2 20 0>;
num-chipselects = <2>;
spidev0: spi@0 {
compatible = "spidev";
reg = <0>;
spi-max-frequency = <57600000>;
};
spidev1: spi@1 {
compatible = "spidev";
reg = <1>;
spi-max-frequency = <57600000>;
};
};
Thanks for your help
Kind Regards,
Diego Caacanova
Hi Diego,
Have you checked if other drivers that are loaded later are changing the pins configurations?
Additionally, you could take a look at the following page for complementary information:
http://free-electrons.com/kerneldoc//latest/devicetree/bindings/pinctrl/fsl,mxs-pinctrl.txt
Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------