Hi all,
Do you know if making a reset on the iMX28 (ball A14 of the IC) I will initialize its internal DC/DC converter?
I've checked the Reference Manual, 11.3.5 Reset Sequence but I'm lost yet
Thank You!
解決済! 解決策の投稿を見る。
DCDC can be restarted as in initial power-up case,
just RESETN will not restart it.
Best regards
igor
I boot the iMX28 from a NAND Flash. This NAND Flash is powered from the iMX28 DCDC_VDDIO line (ball C17).
If the internal DC-DC converter makes a power down for any reason the flash becomes unpowered.
Do you think that I could reboot the iMX28 in this situation?
Thank You!
DCDC can be restarted as in initial power-up case,
just RESETN will not restart it.
Best regards
igor
Hi Jesus
no, RESETN will not initialize DC/DC converter in general reset
is described in sect.11.3.5 Reset Sequence i.MX28 Reference Manual
http://cache.freescale.com/files/dsp/doc/ref_manual/MCIMX28RM.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------