iMX251 diagnostic firmware -blog archive

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX251 diagnostic firmware -blog archive

512 次查看
Suresh
Contributor I

We have created a custom board using the iMX251.

 

Now we have a board with no OS, Drivers, Bootlaoders. We powered the board and JTAG is connected.

 

Can we write a diagnostic firmware to test the on-board peripherals? Assume i will write a C-program to test the memory interface and then cross-compile this code for iMX251 processor and then load in RAM and run the code using JTAG. Is this is possible? Can somebody explain this to me or is there any document which explains this.

 

I have seen the different boot-pins and boot-methods available in TRM and trying to understand this. Can somedoy explain this to me?

标记 (1)
0 项奖励
0 回复数