iMX portrait mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX portrait mode

4,665件の閲覧回数
mariusoctavian
Contributor III

Hello,

I am trying to go in Portrait mode with SABRE iMX6 and 'eGalax Touch Screen,

using Kernel 3.0.35-2508-g54750ff. and uboot u-boot-mx6q-sabresd.bin

The Option Rotate CCW in xorg.conf works only if I comment out the vivante driver.

I really need the vivante inplace, because the media play is acceptable. Without it is terrible.

1. Is there a workaround to rotate and keep vivante in place ?

Section "Device"
    Identifier    "i.MX Accelerated Framebuffer Device"
    Driver        "fbdev"
#    Driver        "vivante"
    Option        "fbdev"        "/dev/fb0"
#    Option        "vivante_fbdev"    "/dev/fb0"
    Option        "Rotate"    "CCW"
EndSection

Second is the evdev touch Axis swap option which does not work, even the

xinput --list-props 11 <cr> reports the swapping setting was committed.

Device 'eGalax Touch Screen':

    Device Enabled (114):    1

    Coordinate Transformation Matrix (115):    1.000000, 0.000000, 0.000000, 0.000000, 1.000000, 0.000000, 0.000000, 0.000000, 1.000000

    Device Accel Profile (232):    0

    Device Accel Constant Deceleration (233):    1.000000

    Device Accel Adaptive Deceleration (234):    1.000000

    Device Accel Velocity Scaling (235):    10.000000

    Evdev Axis Inversion (236):    0, 0

    Evdev Axis Calibration (237):    31935, 284, 33626, 869

    Evdev Axes Swap (238):    1

Thank you.

ラベル(2)
0 件の賞賛
4 返答(返信)

1,601件の閲覧回数
henriroosen
Contributor I

I'm having the same issue: our product will have it's display rotated by 90-degrees.

The vivante driver doesn't seem to support any display rotation and the normal fbdev is not an option performance wise.

Does anyone have some workaround or early code available that enables hardware rotation?

0 件の賞賛

1,601件の閲覧回数
mariusoctavian
Contributor III

Hi,

Does anyone know where the vivante source code drivers are located?

... I found the source in kernel, but there is noting more than meaningless entry points.

Also: I've tried:

echo NN > /sys/class/graphics/fb0/rotate

where NN id 0 1 2 3 4, and works only if the vivante driver is not loaded.

Any success out there. 

0 件の賞賛

1,601件の閲覧回数
Dataedge
Contributor I

Hi all,

about Vivante drivers screen rotation: like you, our product will have it's display rotated by 270-degrees (counter clockwise CCW).

Any news about that ?

0 件の賞賛

1,601件の閲覧回数
mariusoctavian
Contributor III

Rotation touch work around:

Is working with matrix as:

  • xinput set-prop "eGalax Touch Screen" 'Coordinate Transformation Matrix' 0 -1 1 1 0 0 0 0 1

which I place it in ~/.xitinit

0 件の賞賛