Hi,
I was looking on the LCDIF MIPI-DPI for iMX-93 processor. I want to interface a parallel TFT LCD in RGB555 configuration. Anywhere in the datasheet I didn't find the pin multiplexing for RGB DATA (R0-R4, G0-G4, B0-B4) for RGB555 configuration.
Define the pixel color coding to be used by using the dpi_color_coding field in the
DPI_COLOR_CODING register
so for more detailed information, pls refer to the chapter 52.4.2.6 DPI color coding (DPI_COLOR_CODING)
for rgb555, refer to the
https://learn.microsoft.com/en-us/windows/win32/directshow/working-with-16-bit-rgb
should be xRRRRRGGGGGBBBBB
you can refer to the table as below, then connect as xRRRRRGGGGGBBBBB
then choose the register as below