Hello Team,
My customer has sent our imx 8m mini reference design SOM (from the EVK) to PCB manufacturer but they could not achieve the requested 50 Ohms(tolerance 10%) impedance after they careful calculate again, they only can reach to 48 Ohms(tolerance 10%)
Here are the two rise questions, I will appreciate your advice
A. Dose the impedance is 48 Ohms(tolerance 10%) is acceptable?
B. In case the impedance must be 50 Ohms(tolerance 10%), is allowed to adjust the following
The inner copper thickness adjust to 0.5 OZ
The inner line width adjust to 3.7MIL
Please advise back, Thanks in advance
Best regards,
Shai